KEA32 Downloading binary to target...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KEA32 Downloading binary to target...

1,991 Views
cheolminlee
Contributor II

Hi,

I used Codewarrior 10.7.

I use KEA32 but the program can not be downloaded.

Downloading binary to target...

I know that the header file is wrong and I have tried it with other KEA series header files.

Help me...

0 Kudos
Reply
3 Replies

1,911 Views
cheolminlee
Contributor II

Hi,

Thank you for your reply.

I am using KEA32 as a 32pin. Making PCB

When I download the program, I get up to 100%, but 'downloading binary to target ...'

I don't know that...

0 Kudos
Reply

1,911 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi CheolMin Lee

Could you describe more what is the error that you get when you try to download the binary. What do you mean with I have tried it with other KEA series header files.?

You shouldn't change the header file that code warrior generate when you create the project, so please describe more your issue.

Best Regards

Jorge Alcala

0 Kudos
Reply

1,911 Views
mjbcswitzerland
Specialist V

Hi

I believe that S32 Design Studio is what tends to be used with the KEA32 - I don't know that CW10.7 supports programming and debugging it(?)
Try a binary from here in case you think it may be a problem with the binary being used: http://www.utasker.com/kinetis/FRDM-KEAZN32Q64.html

Regards

Mark

0 Kudos
Reply