KEA-128 operation at 3.3v

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KEA-128 operation at 3.3v

1,005 Views
vigneshbalaji
Senior Contributor I

Hi,

     I want to operate the pins of KEA-128 at 3.3v instead of 5v, what are the things to do for it and consequences it has. I have the following questions based on this.

1)Is it recommended to operate KEA-128 pins at 3.3 v instead of 5v?

2)What should i do to operate KEA-128 pins at 3.3 v?

3)What are the consequences of operating KEA-128 pins at 3.3v?

0 Kudos
Reply
1 Reply

932 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hello VIGNESH BALAJI,

  

1)Is it recommended to operate KEA-128 pins at 3.3 v instead of 5v?

Answer: Both 3.3V and 5 can work, because the KEA128 operation voltage is 2.7V to 5.5V.

2)What should i do to operate KEA-128 pins at 3.3 v?

Answer: Just power on the chip with 3.3V.

3)What are the consequences of operating KEA-128 pins at 3.3v?

Answer: No bad consequences, 3.3V is also the normal voltage.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply