KEA 128(i2c of Kea 128) with ISL29023(ambient light sensor)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KEA 128(i2c of Kea 128) with ISL29023(ambient light sensor)

跳至解决方案
1,062 次查看
vignesh_vb_7
Contributor IV

Hi guys,

            Can anyone help me in getting a code for KEA-128 communicating with ISL29023(ambient light sensor) in I2C  ?

1 解答
876 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Vignesh,

There's no kind of this demo for download at present.

However I've attached a template demo which contains I2C driver, so I'd like to suggest that you can use the I2C driver to establish communication with the ISL29023 and you also need to comply the sequence of read and write operation by referring to the ISL29023's datasheet.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

3 回复数
877 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Vignesh,

There's no kind of this demo for download at present.

However I've attached a template demo which contains I2C driver, so I'd like to suggest that you can use the I2C driver to establish communication with the ISL29023 and you also need to comply the sequence of read and write operation by referring to the ISL29023's datasheet.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

876 次查看
vignesh_vb_7
Contributor IV

Thank you very much jeremyzhou :smileyhappy: for sharing the drivers of KEA-128.

0 项奖励
回复
876 次查看
vignesh_vb_7
Contributor IV

Thank you jeremyzhou.I will try with it :smileyhappy:

0 项奖励
回复