KEA 128(i2c of Kea 128) with ISL29023(ambient light sensor)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KEA 128(i2c of Kea 128) with ISL29023(ambient light sensor)

ソリューションへジャンプ
1,029件の閲覧回数
vignesh_vb_7
Contributor IV

Hi guys,

            Can anyone help me in getting a code for KEA-128 communicating with ISL29023(ambient light sensor) in I2C  ?

1 解決策
843件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Vignesh,

There's no kind of this demo for download at present.

However I've attached a template demo which contains I2C driver, so I'd like to suggest that you can use the I2C driver to establish communication with the ISL29023 and you also need to comply the sequence of read and write operation by referring to the ISL29023's datasheet.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
844件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Vignesh,

There's no kind of this demo for download at present.

However I've attached a template demo which contains I2C driver, so I'd like to suggest that you can use the I2C driver to establish communication with the ISL29023 and you also need to comply the sequence of read and write operation by referring to the ISL29023's datasheet.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

843件の閲覧回数
vignesh_vb_7
Contributor IV

Thank you very much jeremyzhou :smileyhappy: for sharing the drivers of KEA-128.

0 件の賞賛
返信
843件の閲覧回数
vignesh_vb_7
Contributor IV

Thank you jeremyzhou.I will try with it :smileyhappy:

0 件の賞賛
返信