KE18F Single Bit ECC Interrupt/Reporting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KE18F Single Bit ECC Interrupt/Reporting

1,337 Views
sean_dvorscak
Contributor III

The KE18F has a mechanism in the FTFE module to generate an interrupt for double bit errors using the FTFE_FERSTAT[DFDIF].

Is there something similar for reporting single bit errors?

Would doing a margin read fill the role of determining single bit errors?

0 Kudos
Reply
1 Reply

1,330 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi sean,

No, there isn't flag which can report single bit error.

You can use margin read to check flash array. But I doubt if it can pick out single error bit. Since it is on the margin level, the error bit  may jump out randomly. Margin check has a certain pattern, for example, write all zero -> all one -> 0x5555aaaa -> 0xaaaa5555. And then change the margin level and do again. 

 

Regards,

Jing

 

0 Kudos
Reply