KE06Z Oscillator not working on custom board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KE06Z Oscillator not working on custom board

1,827件の閲覧回数
stevenlutz
Contributor III

I've just assembled a custom board for a LQFP-44 package KE06Z chip. When I assembled everything, I put a scope on the oscillator to find that it's not oscillating. I used the FRDM-KE06Z as a reference design. This was a preliminary check and I have not actually tried flashing the chip yet. But my main question is if the oscillator should operate prior to flashing being that Xtal and EXTAL are the defaults for the pins 9 and 10 which using. 

Where do the defaults in the datasheet actually come from? are they defauls in the SDK or are they defaults hardcoded in the chip from the factory?


ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,741件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Mark is correct.

If you want to observe the oscillating, please try to flash corresponding program first.

Best Regards,

Robin

0 件の賞賛
返信

1,741件の閲覧回数
mjbcswitzerland
Specialist V

Hi Steven

The crystal oscillator will only start when you load code to program it (in OSC0_CR). It will not oscillate by default, even though the pins default to that mode.

regards

Mark

Complete Solutions and technical support for professional Kinetis developments: http://www.utasker.com/kinetis.html

0 件の賞賛
返信