KE06 EEPROM Emulation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KE06 EEPROM Emulation

1,679 Views
johnec
Contributor I

We are currently using a KE06 device, we need to use EEPROM emulation, is a driver available?

0 Kudos
Reply
1 Reply

1,538 Views
jeremyzhou
NXP Employee
NXP Employee

Hi John,

The EEPROM emulation driver hasn't provided the kind of demo for the KE06, however it can be ported to the KE06 easily.

Please go to download the driver through the link as below.

cache.nxp.com/files/32bit/software_tools/KEAZN8_64_EEE_DEVD.exe?fpsp=1&WT_TYPE=Device%20Drivers&WT_V...​

Hope it hleps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply