KE06 EEPROM Emulation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KE06 EEPROM Emulation

1,679件の閲覧回数
johnec
Contributor I

We are currently using a KE06 device, we need to use EEPROM emulation, is a driver available?

0 件の賞賛
返信
1 返信

1,538件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi John,

The EEPROM emulation driver hasn't provided the kind of demo for the KE06, however it can be ported to the KE06 easily.

Please go to download the driver through the link as below.

cache.nxp.com/files/32bit/software_tools/KEAZN8_64_EEE_DEVD.exe?fpsp=1&WT_TYPE=Device%20Drivers&WT_V...​

Hope it hleps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信