KDS 3.2.0 - issue with linker gone missing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KDS 3.2.0 - issue with linker gone missing

855 次查看
aes_mike
Contributor III

We are trying to migrate an older KL03 KDS project to a new computer and having a strange issue.   Under "properties -> C/C++ build --> Settings --> Tool Settings" the "cross ARM C Linker" has gone missing and not sure what to make of it. 

With the same KDS 3.2.0 environment, we can bring in a K64 project and all is well.

Here are details of the KL03 project:

1. It is using KSDK_1.3.0   library

2. Using KDS 3.2.0.

I am aware that if the build artifact type is set to anything other than executable the linker in the tool settings tab will go away.   And, given that other projects seem to work fine, I think there is something either with KDS installation or the project itself or maybe installed software missing (Help->Installation Details)?

Any advice?

标签 (1)
标记 (2)
0 项奖励
回复
2 回复数

785 次查看
BlackNight
NXP Employee
NXP Employee

Not sure if I can follow, so can you share a screenshot what you see?

0 项奖励
回复

785 次查看
aes_mike
Contributor III

Hi Erich, 

Sorry for the vagueness.  We are working with a customer off-site trying to get them setup with KDS for an older project.  I will try to get more information.  

Thanks!

Mike

0 项奖励
回复