K82: ARM errata 838869 and SysTick handler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K82: ARM errata 838869 and SysTick handler

2,452件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi !

 

I can see _DSB() entry  in almost all interrupt handlers for fix errata case.

 

But not in TickTimerHandler in FreeRTOS port.c:

 

void xPortSysTickHandler(void)
{
   uint32_t ulDummy;

   ulDummy = portSET_INTERRUPT_MASK_FROM_ISR();
   {
   /* Increment the RTOS tick. */
      if (xTaskIncrementTick() != pdFALSE)
      {
         /* Pend a context switch. */
         portNVIC_INT_CTRL_REG = portNVIC_PENDSVSET_BIT;
      }
   }
   portCLEAR_INTERRUPT_MASK_FROM_ISR(ulDummy);

 

// ???

}

 

Even if I unroll all macros, _DSB is not visible.

Or errata is not effect special handlers ?

 

By the way, do you have idea when new SDK will be released  with new FreeRTOS 10.1.0 for K82 ?

Regards,

Eugene

0 件の賞賛
返信
1 返信

1,753件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Eugene,

DSB is used before ISR return only if ISR's last operation is accessing peripheral registers.

Regarding your other question, we don't have a date for the release of the SDK with the new version of FreeRTOS. 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 件の賞賛
返信