K70 UART0 using ISO7816

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K70 UART0 using ISO7816

ソリューションへジャンプ
4,377件の閲覧回数
stephanoschoi
Contributor II

I want to use uart0 for ISO 7816

SIM power is connected to GPIO

SIM reset is connected to GPIO

SIM clock is connected to FTM0_3

SIM Data is connected to UART0 TX

How to initialize uart0 and FTM0_3.

and how to get ATR information.

please help me

ラベル(1)
1 解決策
3,943件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Stephanos,

The attachment includes all the source files for this demo, you may run the "make_new_project.exe" in the folder of "KINETIS_120MHZ_SC\build\iar", and create a project named as "iso7816_demo", and then copy and replace all the files in the folder of "KINETIS_120MHZ_SC\src\projects\iso7816_demo" with the attached one.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

5 返答(返信)
3,943件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Stephanos Choi,

Please kindly refer to the attached ISO7816 demo for details. It is based on TWR-K70F120M.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,943件の閲覧回数
stephanoschoi
Contributor II

I have KINETIS_120MHZ_SC but cannot find the demo.

where is it in KINETIS_120MHZ_SC?

0 件の賞賛
返信
3,943件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

I wrote that demo based on KINETIS_120MHZ_SC, so it is not in the released version.. Please kindly refer to the attached KINETIS_120MHZ_SC.7z.zip for details.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,943件の閲覧回数
stephanoschoi
Contributor II

Thanks Kan

But I cannot down load the file, it is displayed like"Security policy violation detected. The file has been removed."

Please send me the file to e-mail ( [email protected] ).

Have a nice day.

Stephanos

0 件の賞賛
返信
3,944件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Stephanos,

The attachment includes all the source files for this demo, you may run the "make_new_project.exe" in the folder of "KINETIS_120MHZ_SC\build\iar", and create a project named as "iso7816_demo", and then copy and replace all the files in the folder of "KINETIS_120MHZ_SC\src\projects\iso7816_demo" with the attached one.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------