K66 UART FIFO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K66 UART FIFO

1,623 Views
leerollick
Contributor I

Does the UART FIFO require interrupts to be enabled?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,489 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

no. But it would be better to enable interrupt when using FIFO.

59.9.1 Transmit receive data buffer operation.jpg

You can refer the examples in SDK_2.3.0_FRDM-K66F.

SDK_2.3.0_FRDM-K66F.jpg

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply