K65F SDRAM configuration details

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K65F SDRAM configuration details

Jump to solution
2,633 Views
treefrog
Contributor III

Hello!

We've got a TWR-K65F devel board, our custom board will be based on this later and we'll also put an SDRAM to it to satisfy our memory needs. Probably the SDRAM chip will be of different type, size, parameters etc. therefore I'm very focused on understanding all the details of SDRAM interfacing, more precisely SDRAM controller configuration.

I checked this thoroughly:

How-to-access-SDRAM-based-on-K65-SDRAM-controller/ta-p/1129000 

And also generated the SDRAM sample init code by MCUXpresso for TWR85F.

The only detail I don't understand presently is the correct setting of SDRAM_CM0 register. On TWR-K65F the memory chip has 4 banks, 2048 rows and 256 columns, and the data size is 32-bits (4 * 2048 * 256 * 4 = 8MB). Because of the 32-bit data size the 2 lowest bits of address are ignored. In the MCUXpresso code and in the referred PDF the memory base address is 0x80000000.

I simply don't understand how SDRAM_CM0 value of 0x007C0001 is got. More accurately, the 14-bit wide BAM (Base Address Mask) field is ambiguous to me, and I want to be able to calculate it by myself (remember, we'll likely adapt a different SDRAM chip).

I only have one theory for calculation (frankly, I also don't believe this is right): 0x7C is binary 0111 1100. The 2 lowest bits are reserved, there 0, by "eliminating" them 11111 remains. This is decimal 31 which is quite close to the chip data size (32 bits).

Could you please someone clarify how to calculate CM0:BAM value knowing the base address (0x80000000), column width, row number, bank number, data size?

 

0 Kudos
Reply
1 Solution
2,619 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi treefrog,

Actually, BAM means how many 256k size memory space is used by the SDRAM. If SDRAM_CM0=0x7c0001, the BAM is 0x1f. So, the address range is 256k*(31+1)=8M.

 

Regards,

Jing

View solution in original post

0 Kudos
Reply
2 Replies
2,620 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi treefrog,

Actually, BAM means how many 256k size memory space is used by the SDRAM. If SDRAM_CM0=0x7c0001, the BAM is 0x1f. So, the address range is 256k*(31+1)=8M.

 

Regards,

Jing

0 Kudos
Reply
2,616 Views
treefrog
Contributor III

Many  thanks, it's quite simple.

(I think it'd worth adding this little bit of info to the CPU manual)

0 Kudos
Reply