K64 SPI 1 Baudrate through MCUConfig Tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K64 SPI 1 Baudrate through MCUConfig Tool

ソリューションへジャンプ
1,675件の閲覧回数
ahmedhrabi
Contributor IV

Hi All, 

I'am working on the K64 with the MCUconfigTool. The bus Clock value is 50.381Mhz, and i'am using it to generate the SPI1 Clock. The Desired Baudrate of the SPI is 350000. 

Here's my McuConfigTool config : 

 

SPI1 SCK Pin : 

Capture spi 1 pin.PNG

SPI1 Periph config : 

Periph spi 1 config.PNG

With this configuration the measured generated clock of the SPI 1 (SCK) is always 12.59Mhz, even when i chaned the desired baudrate to other values i always get 12.59Mhz. 

PS : I have tried the same conf for the SPI 0 and it works correctly (The generated SCK is 350 000 Hz). 

Best Regards, 

Ahmed HRABI. 

1 解決策
1,549件の閲覧回数
ahmedhrabi
Contributor IV

The selected Ctar was wrong. Resolved problem 

元の投稿で解決策を見る

1 返信
1,550件の閲覧回数
ahmedhrabi
Contributor IV

The selected Ctar was wrong. Resolved problem