K64 & K66 family devices support for NOR Flash & PSRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K64 & K66 family devices support for NOR Flash & PSRAM

2,841 Views
praveenkajjam
Contributor II

Hello,

Will K64 & K66 family devices support the interface for NOR Flash & PSRAM over the FlexBus? I am not able to find any design reference in Reference Manual. We have a requirement to use the MT38W1011A90YZQXZI.XB8

combo memory in our design from Micron.

Thanks & Regards,

Praveen Kajjam.

Labels (1)
Tags (1)
4 Replies

2,531 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Praveen,

The TWR-MEM module includes a SRAM device, and it can work with other tower boards likes the TWR-K60D100 to read or write the SRAM chip.

TWR-MEM:

 http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-MEM

TWR-K60D100:

TWR-K60D100M|Tower System Board|Kinetis MCUs|NXP 


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,531 Views
praveenkajjam
Contributor II

Hello Jeremyzhou,

            My question is not regarding SRAM. I want to interface NOR Flash and PSRAM over FlexBus. Planning to use this chip from Micron. Will K64& K66 support interface to this device over FlexBus?

Thanks & Regards,

Praveen Kajjam

0 Kudos
Reply

2,531 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Praveen,

The FlexBus interface can support the single NOR Flash or PSRAM device, however about the MT38W1011A90YZQXZI, the FlexBus interface will fail to support the some operation with the NOR Flash and PSRAM simultaneously.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,531 Views
praveenkajjam
Contributor II

Hello Jeremy,

            Thanks for your confirmation. Anyhow we are going to use either NOR flash or PSRAM as the address & data bus is multiplexed between them. But I did pin comparison of the combo memory chip with the FlexBus of K64, I found that it perfectly meets the interface requirements for PSRAM but not fully meets interface requirements for NOR Flash. Refer the below table for the same. Cells highlighted (NOT_WP, NOR_RP, NOR_CLK and NOR_WAIT) in orange are not supported from FlexBus. Any guidance on how to handle them (Especially NOR-WAIT)? If you have any reference schematics with NOR Flash interface that will be useful.

 

Micron -NOR+PSRAM

Freescale-K64

MT38W1011A90YZQXZI.XB8

MK64FN1M0VLQ12

NOR FLASH

PSRAM

FB_AD0

A_00

A_00

FB_AD1

A_01

A_01

FB_AD2

A_02

A_02

FB_AD3

A_03

A_03

FB_AD4

A_04

A_04

FB_AD5

A_05

A_05

FB_AD6

A_06

A_06

FB_AD7

A_07

A_07

FB_AD8

A_08

A_08

FB_AD9

A_09

A_09

FB_AD10

A_10

A_10

FB_AD11

A_11

A_11

FB_AD12

A_12

A_12

FB_AD13

A_13

A_13

FB_AD14

A_14

A_14

FB_AD15

A_15

A_15

FB_AD16

DQ_00

DQ_00

FB_AD17

DQ_01

DQ_01

FB_AD18

DQ_02

DQ_02

FB_AD19

DQ_03

DQ_03

FB_AD20

DQ_04

DQ_04

FB_AD21

DQ_05

DQ_05

FB_AD22

DQ_06

DQ_06

FB_AD23

DQ_07

DQ_07

FB_AD24

DQ_08

DQ_08

FB_AD25

DQ_09

DQ_09

FB_AD26

DQ_10

DQ_10

FB_AD27

DQ_11

DQ_11

FB_AD28

DQ_12

DQ_12

FB_AD29

DQ_13

DQ_13

FB_AD30

DQ_14

DQ_14

FB_AD31

DQ_15

DQ_15

FB_A16

A_16

A_16

FB_A17

A_17

A_17

FB_A18

A_18

A_18

FB_A19

A_19

A_19

FB_A20

A_20

A_20

FB_A21

A_21

A_21

FB_A22

A_22

NA

FB_A23

NA

NA

FB_A24

NA

NA

FB_A25

NA

NA

FB_A26

NA

NA

FB_A27

NA

NA

FB_A28

NA

NA

FB_A29

NA

NA

FB_CS0

NOR_CE

PSRAM_CE

FB_CS1

NA

NA

FB_CS2

NA

NA

FB_CS3

NA

NA

FB_CS4

NA

NA

FB_CS5

NA

NA

FB_OE

NOR_OE

PSRAM_OE

FB_RW

NOR_WE

PSRAM_WE

FB_BE_0_7

NA

NA

FB_BE_8_15

NA

NA

FB_BE_16_23

NA

PSRAM_LB

FB_BE_24_31

NA

PSRAM_UB

FB_ALE

NOR_ADV

NA

NA

NOR_WP

NA

NA

NOR_RP

NA

NA

NOR_CLK

NA

NA

NOR_WAIT

NA

 

 

Thanks & Regards,

Praveen Kajjam

0 Kudos
Reply