K61 part internal flash size

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K61 part internal flash size

1,410 次查看
nanjundam
Contributor II

Hi,

I have a requirement to use the micro controller MK61FX512VMJ12.

I'm bit confused with its part break up and memory size.

As per the part break up it says it has a program flash size of 512KB.

Does it mean it has the Flex NVM and Flash memory as total size of 512KB or indivially there is 512KB of Flex NVM and 512KB of Flash memory ?

There is a mention of SRAM for this device. How do I find the size of this interanl SRAM for the given device.

Please help us at the earliest.

Thanks & Regards,
Nanjunda M

标记 (1)
0 项奖励
回复
1 回复

1,295 次查看
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear Nanjunda M,

This device have:

  • 512 KB of Flash
  • 512 KB FlexMem
  • 128 KB RAM
  • 16 KB FlexRAM

In the Data sheet in the first page you will find the  Memories and memory interfaces.

you can have some information there about the size of the memories and there are specific sections for each one.

hope this helps.

have a great day

BR

Jonathan

0 项奖励
回复