K60 CAN message buffer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60 CAN message buffer

3,777 Views
tenfy
Contributor I

     I am implementing the CAN module of K60, As known, the CAN module has 16 message buffers which can be configured as receive buffer and transmit buffer.

     Now I want to configure 8 message buffers as transmit buffer,and call them "hard-buffer". It means that I can use the 8 transmit message buffers to transmit my CAN messages.

     When I begin to send my CAN messages, I need to judge which transmit message buffer is empty, but I don't know how to judge it.

     My questions are that:

     1:how to jude whether a transmit message buffer is empty;

     2:Is it necessary to use the 8 transmit message buffers to transmit CAN messages simultaneously.

                                                                                                                                       Thanks!

                                                                                                                                  yours:tenfyzhang

Labels (1)
Tags (2)
0 Kudos
Reply
4 Replies

3,378 Views
Monica
Senior Contributor III

Hello Tenfy,

How did you find those answers? Were they helpful?

Please keep us posted :smileywink:

Regards,

Monica.

0 Kudos
Reply

3,378 Views
tenfy
Contributor I

Hello,Moniaca Arvizu

I am sorry to tell you that I can't understand what's your meaning about these words as follows.can you make it in detail.

Thanks!

在 2013-07-25 08:28:36,"Monica Arvizu" <[email protected]> 写道:

|

|

|

|

K60 CAN message buffer

reply from Monica Arvizu in Kinetis Microcontrollers - View the full discussion

Hello Tenfy,

How did you find those answers? Were they helpful?

Please keep us posted

Regards,

Monica.

Reply to this message by replying to this email, or go to the message on Freescale Community

Start a new discussion in Kinetis Microcontrollers by email or at Freescale Community

|

|

0 Kudos
Reply

3,378 Views
Monica
Senior Contributor III

Hello Tenfy, I'm sorry for making it confusing. I just wanted to know if the answer that Wiping gave was the one you needed.

Best regards,

Monica

0 Kudos
Reply

3,378 Views
weapon
Senior Contributor I

Hi Tenfy,

1. You can check the CODE field of the message buffer.

Transmit data frame unconditionally once. After transmission, the MB automatically returns to the INACTIVE state.

Transmit remote request frame unconditionally once. After transmission, the MB automatically becomes an Rx Empty

MB with the same ID.

2. Not necessary.

If two or more MBs are prepared to transmit frames, the arbitration process will be started to check all prepared MBs to get "arbitration winner". Only the winner can send frames one time.

Best Regards

Weiping