K60 120Mhz ADC2 ,ADC3 Channel assignment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60 120Mhz ADC2 ,ADC3 Channel assignment

1,246 Views
sabinbercovich
Contributor I

Hi all

I am using the K60 120Mhz 1M0 and i don't find the ADC2 and ADC3 Connections/channel assignment table in the reference menual like the tables for ADC0 and DC1

Can any one direct me to find this tables

thanks

Sabin

Labels (1)
0 Kudos
Reply
1 Reply

1,075 Views
perlam_i_au
Senior Contributor I

You can use the ADC1 table as reference for ADC2 and ADC3, in order to do not replicate the same table in documentation only one has been included.


Have a nice day :P,
Perla

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply