K22FN512 UART FIFO Depth

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K22FN512 UART FIFO Depth

1,706 Views
derekcook
Senior Contributor I

Hello, 

In the reference manual I am having a hard time finding out information on FIFO depth for this microcontroller. I see how to define FIFO depth in the UARTx_PFIFO, but does each UART0 and UART1 allow the same FIFO depth. 

I know on the KV31 UART0 is much deeper than UART1 - I just wanted to check if this is the same for the K22 or if both UARTs can be defined the max depth - Just want to be sure my design is correct.

Labels (2)
2 Replies

1,564 Views
mjbcswitzerland
Specialist V

Hi Derek

pastedImage_1.png

Regards

Mark

0 Kudos
Reply

1,564 Views
derekcook
Senior Contributor I

Thanks Mark - I didn't see that in the reference manual. That helped me out.