K22(MK22FN512CAP12R) using ISO 7816

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K22(MK22FN512CAP12R) using ISO 7816

1,567件の閲覧回数
yaochiayang
Contributor I

Hi all,

for ISO7816, three pins are used for communication.

CLK, I/O and RST.

I/O

I will connect I/O with UART0_TX, for I could see in some document UART_TX could be configured to I/O pin for 7816 standard.

also, UART0 are the only one which supports ISO7816 in K22 120MHz.

RST

i will connect RST to UART0_RTS_b.

CLK

i see this information in the forum as well. CLK is suggested to tie with FTM.

i am gonna connect this with FTM0_CH5. is this feasible?

as far as i learn from the reference manual, it seems configurable though.

is the way connection gonna work for SW?

thanks,

Lawrence

ラベル(1)
0 件の賞賛
返信
1 返信

1,181件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Lawrence,

I am sorry, but the ISO7816 RST signal is a reset signal, not the function of UART RTS(Request to send), so if you connected RST to UART0_RTS_b, you should configure this pin as GPIO function, not the UART0_RTS_b function.

Hope that helps,


Have a great day,
Kan

Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信