K22 ADC Calibration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K22 ADC Calibration

1,536件の閲覧回数
sbranover
Contributor I

When non volatile memory is available is it recommended to store and reload the ADC calibration values or is it better to run the auto calibration at every reboot?

We are also storing calibration values for circuitry external to the ADC for which the calibration needs to be preformed in a lab.

ラベル(1)
0 件の賞賛
返信
1 返信

1,435件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

pastedImage_1.png

You would better run the auto calibration at every reboot. Because some factors ,such as temperature, will influence the  the calibration value. So the fixed value will influence the ADC's preciseness.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信