K20‘ s Can bus can not normally start

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K20‘ s Can bus can not normally start

1,511 Views
songtao8940
Contributor I

6Y{KPUX1CSNJMU]6ZN6OO4R.png

As shown in the figure, now can bus program can not normally start, what is the requirement for the clock,plese help me

0 Kudos
Reply
2 Replies

1,421 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

It need to enable the FlexCAN module clock at SIM_SCGC6[FLEXCAN0] bit or SIM_SCGC3[FLEXCAN1] bit at first.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,421 Views
songtao8940
Contributor I

Thank you, now come to the conclusion that indeed the clock problem

0 Kudos
Reply