It is posible implement software Flow Control (Xon/Xoff) over MKL46Z?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

It is posible implement software Flow Control (Xon/Xoff) over MKL46Z?

2,734 Views
dhernandez-m
Contributor I

Hi all,  Sorry if i am  using bad English.

  I am using UART Polled communication with the host ( Putty) over MKL46Z but i can not implement Software Flow Control (Xon/XOFF). It is posibble ? Below show the code i use to do communication task

#include "MKL46Z4.h"
#include "TxRxQueues.h"
#define UART_BUFF_SIZE (10)


char RxQBuffer[UART_BUFF_SIZE], TxQBuffer[UART_BUFF_SIZE];
struct qRecord RxQueue, TxQueue;


void UART_Init()
{
     //clock init
    init_Queue(&RxQueue, RxQBuffer, UART_BUFF_SIZE);
    init_Queue(&TxQueue, TxQBuffer, UART_BUFF_SIZE);

    SIM->SCGC4 |= SIM_SCGC4_UART2_MASK; /* Enable Clock to UART2*/
    // PTA1 -> ALT3 = UART2_RX
    // PTA2 -> ALT3 = UART2_TX
    SIM->SCGC5 |= SIM_SCGC5_PORTE_MASK; /* Enable Clock to PORTA*/
    PORTE->PCR[16] |= PORT_PCR_MUX(3UL);  /* Pin PTA1 is alt2 (UART)*/
    PORTE->PCR[17] |= PORT_PCR_MUX(3UL);  /* Pin PTA2 is alt2 (UART) */

    UART2->C2 &= !UART_C2_TE_MASK;   /* disable transmitting*/
    UART2->C2 &= !UART_C2_RE_MASK;   /* disable receiving */

    UART2->BDH |= UART_BDH_SBR(0);         /*set value of SBR to BDH (it is the first divider)*/
    UART2->BDL |= UART_BDL_SBR(0x185);        /*set value of SBR to BDL 26*/
    UART2->BDH &= !UART_BDH_SBNS_MASK;   /*set value of  SBNS (0 - one bit, 1- two bits) */

    UART2->C1 &= !UART_C1_M_MASK;            /* M selects between 8 and 9 bits data MODE*/
    UART2->C1 &= !UART_C1_PE_MASK;            /* PE - parity enable (0 - no hardware parity)*/

        //UART2->C2 |= UART2_C2_TIE_MASK;            /* enable interrupt*/
        //UART2->C2 |= UART2_C2_RIE_MASK;

    UART2->C2 |= UART_C2_TE_MASK;   /* enable transmitting*/
    UART2->C2 |= UART_C2_RE_MASK;   /* enable receiving */

}
void Send(uint8_t message)
{
    // Send message
        UART2->D= message;
        // Wait for transfer complete
        while(!(UART2->S1 & UART_S1_TDRE_MASK)){}
        //while(!(UART2->S1 & UART_S1_TC_MASK)){}
}


char getChar() {
    char character;
    int success;

    do {
        __asm("CPSID I");
        success = dequeue(&character, &RxQueue);
        __asm("CPSIE I");
    } while (!success);

    return character;
}

Labels (1)
0 Kudos
Reply
2 Replies

2,624 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Diego,

KL46 can support software flow control. Please refer to this case link https://community.nxp.com/message/511094 

KL26 UART port is same to KL46. Hope this can help you.

Regards,

Jing

0 Kudos
Reply

2,624 Views
mjbcswitzerland
Specialist V

Hi

KL46 XON/XOFF SW and RTS/CTS HW flow control are included in the uTasker project - see the open source link below and the UART document: http://www.utasker.com/docs/uTasker/uTaskerUART.PDF

Note that XON/XOFF flow control is implemented at the driver level and not in the UART HW.

Regards

Mark

Complete Kinetis solutions for professional needs, training and support: http://www.utasker.com/kinetis.html
Kinetis KL25, KL26, KL27, KL28, KL43, KL46, KL82
- http://http://www.utasker.com/kinetis/FRDM-KL25Z.html
- http://www.utasker.com/kinetis/TWR-KL25Z48M.html
- http://www.utasker.com/kinetis/FRDM-KL26Z.html
- http://www.utasker.com/kinetis/TEENSY_LC.html
- http://www.utasker.com/kinetis/FRDM-KL27Z.html
- http://www.utasker.com/kinetis/Capuccino-KL27.html
- http://www.utasker.com/kinetis/FRDM-KL28Z.html
- http://www.utasker.com/kinetis/FRDM-KL43Z.html
- http://www.utasker.com/kinetis/TWR-KL43Z48M.html
- http://www.utasker.com/kinetis/FRDM-KL46Z.html
- http://www.utasker.com/kinetis/TWR-KL46Z48M.html
- http://www.utasker.com/kinetis/FRDM-KL82Z.html

uTasker: supporting >1'000 registered Kinetis users get products faster and cheaper to market

Request Free emergency remote desk-top consulting at http://www.utasker.com/services.html

Open Source version at https://github.com/uTasker/uTasker-Kinetis

0 Kudos
Reply