Issue with sdcard in kinetis k70 tower board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue with sdcard in kinetis k70 tower board

1,718 Views
sameerarvikar
Contributor III

Hello,

I am 2 TWR-K70F120M board

In one sdcard is working ,and other its not working

following is the output for mmc info command

Device: FSL_SDHC
Manufacturer ID: 3
OEM: 5344
Name: SL16G
Tran Speed: 25000000
Rd Block Len: 512
SD version 2.0
High Capacity: Yes
Capacity: 15931539456
Bus Width: 1-bit

In the working tower board ,its showing

Bus Width: 4-bit
rest data is same

What might be the issue ,is this  problem  there with the other k70 tower boards,

How to rectify ?

0 Kudos
Reply
3 Replies

1,568 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Could you please provide the TWR-K70F120M board hardware version info?
If both boards with the same hardware version?

pastedImage_1.png


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,568 Views
sameerarvikar
Contributor III

Hi,

Both have same version sch-27166 Rev B1

0 Kudos
Reply

1,568 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Sorry for the later reply.

I checked the system record, there without related info before.

Please check here to warranty replacement that issued TWR-K70F120M board. Thanks.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply