Is there a Mil-Spec version of the KL43P64M48SF6 processor?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a Mil-Spec version of the KL43P64M48SF6 processor?

3,143件の閲覧回数
spflanze
Contributor I

I am looking for ultra low power in Mil-Spec. I need 80uA/MHz or less.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,281件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Stephen Pflanze,

Regarding to the low-power consumption level, the KL43 can down to 54uA/MHz in very low power run mode.

And you can learn the more information from the attachment.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,281件の閲覧回数
spflanze
Contributor I

I still need to know if this processor is available in a Mil-Spec version. I did not see any information about Mil-Spec in the PDF attached to the message on your website.

0 件の賞賛
返信