Is the MK60FN1M0VLQ12 upper compatible with MK20FN1M0VLQ12?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is the MK60FN1M0VLQ12 upper compatible with MK20FN1M0VLQ12?

961 次查看
isaotakashima
Contributor IV

I want to use the MK60FN1M0VLQ12 if need Ethernet function, otherwise I want to use MK20FN1M0VLQ12.
Then I was compare the following Signal Multiplexing and Pin Assignments.
- The 8.2 K20 Signal Multiplexing and Pin Assignments of MK20FN1M0VLQ12 data sheet (K20P144M120SF3 Rev 5)
- The 8.2 K60 Signal Multiplexing and Pin Assignments of MK60FN1M0VLQ12 data sheet (K60P144M120SF3 Rev 5)


As a result, the MK60FN1M0VLQ12 is upper compatible with MK20FN1M0VLQ12 except PTA6.
According to the 8.2 K20 Signal Multiplexing and Pin Assignments, we can assign the PTA6 of the MK20FN1M0VLQ12 as CLKOUT if set PORTA_PCR6[MUX]=5.
But the MK60FN1M0VLQ12 does not have this feature.
I cannot find out that how to assign PTA6 as CLKOUT.
Can we assign the PTA6 of the MK20FN1M0VLQ12 as CLKOUT?

Please advise as soon as possible.

Best regards,
Takashima

标签 (1)
标记 (4)
0 项奖励
回复
2 回复数

679 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Isao

You only can use the PTC3 as a CLKOUT


Have a great day,
Vicente

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

679 次查看
DavidS
NXP Employee
NXP Employee

Hi Isao,

Please look at following post as I think it will answer your question.

Tower BSP/PSP for MK60DX256VMD10 ?

Regards,

David

0 项奖励
回复