Is the ARM PRIMASK LSB used by the KL17 hardware?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is the ARM PRIMASK LSB used by the KL17 hardware?

817 Views
rickstuart
Contributor V

I was wondering, is the ARM PRIMASK least significant bit (controllable by using CPSID i or CPSIE i or __disable_irq() or __enable_irq()) ever used by the KL17's hardware?  Specifically, does the KL17 hardware use the PRIMASK LSB to control the inhibiting of interrupts?

If not, how does the KL17 inhibit interrupts - for example, when the KL17 is in an interrupt it disables that interrupt so as not to cause an infinite number of interrupt calls.

-thanks

0 Kudos
Reply
0 Replies