Is it possible to develop the KW30 in KDS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to develop the KW30 in KDS?

Jump to solution
2,024 Views
Lupo
Contributor III

It seems that the stack installed by the "Kinetis KW40Z Connectivity Software" must be compiled in IAR...
but IAR EWARM is very expensive...
Is there a way to develop in Kinetis Design Studio?
Thanks also for any explanation of this choice.

Kinetis KW40Z Connectivity Software

Labels (1)
0 Kudos
Reply
1 Solution
1,878 Views
miduo
NXP Employee
NXP Employee

Hi,

Actually the reason that the KDS does not support the "Kinetis KW40Z Connectivity Software" is beause the BLE stack is not supported. Unfortunately there are no plans for having the KDS supporting the BLE stack, so the only IDE supported right now is IAR Workbench.

View solution in original post

0 Kudos
Reply
2 Replies
1,879 Views
miduo
NXP Employee
NXP Employee

Hi,

Actually the reason that the KDS does not support the "Kinetis KW40Z Connectivity Software" is beause the BLE stack is not supported. Unfortunately there are no plans for having the KDS supporting the BLE stack, so the only IDE supported right now is IAR Workbench.

0 Kudos
Reply
1,878 Views
Lupo
Contributor III

Thanks Fang Li, I understand :smileysad:

0 Kudos
Reply