Internal Vref for ADC in MK10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Internal Vref for ADC in MK10

1,874件の閲覧回数
ssarathkumar916
Contributor II

Hi,

We are using MK10DX256xxx7 controllers. and We use Rowley cross works IDE for programming. 

We want to use 1.2V Internal VREF for ADC.

As per datasheet,we tried setting ADC_SC2->REFSEL 

and VREF_SC->VREFEN

we probed VREF_OUT pin using Oscilloscope, but  no voltage got generated. 

Please guide us to generate internal 1.2V VREF.

Please share any code or schematics for reference.

Thanks,

Sarathkumar S

#MK10DX256xxx7 

 #ADC

 #Internal Verf

ラベル(1)
1 返信

1,750件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello [email protected]‌

I suggest you to leave the bit REFSEL of the register ADC_SC2 as 0x01.

For the VREF status a control register please set 0x01 at the following bits: VREFEN, REGEN, ICOMPEN and MODE_LV.

 

Please let me know if this is helpful.

Best regards,

Omar