Interface MPC860 with Micron SDRAM [MT48LC8M16A2TG]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interface MPC860 with Micron SDRAM [MT48LC8M16A2TG]

1,404 Views
balaji76
Contributor I

Dear All,

         I am using the processor MPC860 and interface with SDRAM [8MB]. Using external clock[66MHz],  the initialization for SDRAM and chip select CS1.

writemmr BR00xFFF00001 # BR0 - Boot Flash starts at 0xFFF00000
writemmr OR00xFFF00074 # OR0 - SIZE OF THE BOOT FLASH IS 1MBYTE

writemmr BR10x00000081 # BR1 - SDRAM starts at 0x00000000
writemmr OR10xFF000800 # OR1 - SIZE OF THE SRAM IS 16MBYTEs

#writemmr BR70x00000801 # BR2 - ram starts at 0x20000401
#writemmr OR70xFFF00074

I commented BR7 and OR7 for RAM functionality and enable the SDRAM. Load the configure file for erase and programming. when try to erase the flash, only chip select 1 signal is correct. other than that SD_WE#, OE# signals are tri-state. I don't know why it is coming like that? Bank Select configured for A7 and A8.

Can you check it and mail me?         I am eager to waiting for your reply.

Thanking you,

Regards

Balaji

0 Kudos
Reply
1 Reply

1,226 Views
alexander_yakov
NXP Employee
NXP Employee

The initialization of only BR1 and OR1 is not enough to initialize SDRAM on chip select CS1.

Please refer to application note AN2066 for MPC8xx SDRAM interface inplementation

http://cache.freescale.com/files/netcomm/doc/app_note/AN2066.pdf

0 Kudos
Reply