Initialize TWR-MEM MMEM with Kinetis

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Initialize TWR-MEM MMEM with Kinetis

Jump to solution
1,998 Views
terrybiberdorf
Contributor II

I'm having problems trying to initialize the MMEM on my TWR-MEM board.

I'm using the following init code:

#define MRAM_START_ADDRESS (*(volatile unsigned char*)(0x60000000))

void FlexBusInit()

{

    SIM_SCGC7 |= SIM_SCGC7_FLEXBUS_MASK; // Enable the clock to the FlexBus

    SIM_CLKDIV1 |= SIM_CLKDIV1_OUTDIV3(0x0); //FlexBus Clock not divided

   

    // Set the GPIO ports clocks

    SIM_SCGC5 = SIM_SCGC5_PORTA_MASK | SIM_SCGC5_PORTB_MASK | SIM_SCGC5_PORTC_MASK |

    SIM_SCGC5_PORTD_MASK | SIM_SCGC5_PORTE_MASK;

    PORTB_PCR11 = PORT_PCR_MUX(5); // fb_ad[18]

    PORTB_PCR16 = PORT_PCR_MUX(5); // fb_ad[17]

    PORTB_PCR17 = PORT_PCR_MUX(5); // fb_ad[16]

    PORTB_PCR18 = PORT_PCR_MUX(5); // fb_ad[15]

    PORTC_PCR0 = PORT_PCR_MUX(5); // fb_ad[14]

    PORTC_PCR1 = PORT_PCR_MUX(5); // fb_ad[13]

    PORTC_PCR2 = PORT_PCR_MUX(5); // fb_ad[12]

    PORTC_PCR4 = PORT_PCR_MUX(5); // fb_ad[11]

    PORTC_PCR5 = PORT_PCR_MUX(5); // fb_ad[10]

    PORTC_PCR6 = PORT_PCR_MUX(5); // fb_ad[9]

    PORTC_PCR7 = PORT_PCR_MUX(5); // fb_ad[8]

    PORTC_PCR8 = PORT_PCR_MUX(5); // fb_ad[7]

    PORTC_PCR9 = PORT_PCR_MUX(5); // fb_ad[6]

    PORTC_PCR10 = PORT_PCR_MUX(5); // fb_ad[5]

    PORTD_PCR2 = PORT_PCR_MUX(5); // fb_ad[4]

    PORTD_PCR3 = PORT_PCR_MUX(5); // fb_ad[3]

    PORTD_PCR4 = PORT_PCR_MUX(5); // fb_ad[2]

    PORTD_PCR5 = PORT_PCR_MUX(5); // fb_ad[1]

    PORTD_PCR6 = PORT_PCR_MUX(5); // fb_ad[0]

   

    PORTB_PCR20 = PORT_PCR_MUX(5); // fb_ad[31] used as d[7]

    PORTB_PCR21 = PORT_PCR_MUX(5); // fb_ad[30] used as d[6]

    PORTB_PCR22 = PORT_PCR_MUX(5); // fb_ad[29] used as d[5]

    PORTB_PCR23 = PORT_PCR_MUX(5); // fb_ad[28] used as d[4]

    PORTC_PCR12 = PORT_PCR_MUX(5); // fb_ad[27] used as d[3]

    PORTC_PCR13 = PORT_PCR_MUX(5); // fb_ad[26] used as d[2]

    PORTC_PCR14 = PORT_PCR_MUX(5); // fb_ad[25] used as d[1]

    PORTC_PCR15 = PORT_PCR_MUX(5); // fb_ad[24] used as d[0]

   

    PORTB_PCR19 = PORT_PCR_MUX(5); // fb_oe_b

    PORTC_PCR11 = PORT_PCR_MUX(5); // fb_rw_b

    PORTD_PCR1 = PORT_PCR_MUX(5); // fb_cs0_b

    PORTD_PCR0 = PORT_PCR_MUX(5); // fb_ale

   

    FB_CSAR0 = (unsigned int)&MRAM_START_ADDRESS; //Set Base address

   

    FB_CSCR0 = ( (FB_CSCR_PS(1))     // 8-bit port

            | (FB_CSCR_AA_MASK)     // auto-acknowledge

            | (FB_CSCR_WS(0x6)) );     // 2 wait states

    FB_CSMR0 = ( (FB_CSMR_BAM(0x7)) //Set base address mask for 512K address space

            | (FB_CSMR_V_MASK) );      //Enable cs valid signal

}

But after I complete this API call I found that I only have access to every other 16K block of data.

0x60000000 - 0x60001FFF -> work fine

0x60002000 - 0x60003FFF -> does not work

0x60004000 - 0x60005FFF -> work fine

0x60006000 - 0x60007FFF -> does not work

-------

0x6007C000 - 0x6007DFFF -> works fine

0x6007E000 - 0x6007FFFF -> does not work

Any suggestions?

Thanks

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,855 Views
terrybiberdorf
Contributor II

After receiving a call from my Atmel FAE,  the fix is to remove the J16 jumper.

Somehow the CPLD has corrupting the FlexBus communication.

Thanks Brad.

View solution in original post

0 Kudos
Reply
2 Replies
1,855 Views
terrybiberdorf
Contributor II

I forgot to add, I attempted this code on three tower configurations systems: TWR-K60N512, TWR-K60D100M and a TWR-K70F120M

0 Kudos
Reply
1,856 Views
terrybiberdorf
Contributor II

After receiving a call from my Atmel FAE,  the fix is to remove the J16 jumper.

Somehow the CPLD has corrupting the FlexBus communication.

Thanks Brad.

0 Kudos
Reply