ISSUE WITH MSCAN KEAZ128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ISSUE WITH MSCAN KEAZ128

752 Views
DanielR21
Contributor I

Good day to everyone, 

I'm developing a dispositive in order to obtain data from vehicles trough CAN protocol, I'm using a KEAZ128 development board, I used the examples in order to import libraries for SPI initialization. Now I'm testing it with an Arduino in order to simulathe vehicle with a MCP2515 module, a few weeks ago it worked, now I don't even know if the transceiver chip in turned on. 

The supply of the microcontroller is 12V and Headers of J107 1-2 are connected. 

Someone could help me in order to obtain a solution?

Note: I can't attach the code due to privacy developers

0 Kudos
Reply
0 Replies