INTERFACE MK60N512 WITH SD CARD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

INTERFACE MK60N512 WITH SD CARD

1,604件の閲覧回数
franticcarlitos
Contributor II

Hi,

i want to interface kinetis microcontroller mk60n512 with SD card.

30 ohms series resistor on interfacing signals (D0,D1,D2,D3,DCLK,CMD...) with mcu are needed? I've read that that the baud rate of that signals is 200Mbps using 4 parallel data lines.

How I could find the pcb design guideline for this kind of interface?

Any information about that subject is appreciated.

Thanks

0 件の賞賛
返信
2 返答(返信)

1,383件の閲覧回数
BlackNight
NXP Employee
NXP Employee

I recommend too to have a look at existing designs and boards, as pointed out by Hui_Ma. In case you are looking as well for a software project for the TWR-K60 SD-Card: FatFs with Kinetis | MCU on Eclipse

I hope this helps.

1,383件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I would recommend customer to refer TWR-K60N512 board design, which include SD card design.

TWR-K60N512 board resouce (hardware design files and schematics) could be download from below link:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-K60N512&fpsp=1&tab=Design_Tools_T...

Wish it helps.