IEEE 1588 PTP on FRDM K64F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IEEE 1588 PTP on FRDM K64F

2,081 Views
rolandkohari
Contributor I

I am working with multiple camera system (computer vision), and I would like to use FRDM K64F to sync the CAN,GPS,IMU datas with the camera clocks via IEEE 1588 ptp ethernet protocol. Moreover I want to provide trigger for the cameras in every 40ms. Does anybody have experiencies to configure this protocol?

0 Kudos
Reply
1 Reply

1,620 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

There is an application note AN4332 about IEEE1588 PTP application with Kinetis K60 product.

Related software please check with our third partner IXXAT.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply