IAR can't set breakpoints using i-link on MK02

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IAR can't set breakpoints using i-link on MK02

1,782件の閲覧回数
bruceweyrauch
Contributor I

I'm not sure if this is a better question for IAR or this forum, but I can't seem to get breakpoints to work while debugging my code for the MK02 using C-Spy.  I have attached the console output from a debug session.  I always get the same error - Discarded breakpoint of type STD_CODE2, unknown to the current driver.  but earlier in the log it shows that there are Debug resources: 6 instruction comparators, 4 data watchpoints.

 

I'm thinking I must have something configured wrong, but I can't figure it out.

Original Attachment has been moved to: I-Jet-debug-log.zip

ラベル(1)
0 件の賞賛
返信
0 返答(返信)