I'm trying to communicate at 2.5Mbps using uart1 on mk10d.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I'm trying to communicate at 2.5Mbps using uart1 on mk10d.

1,312件の閲覧回数
tj_P
Contributor I

I want to use uart1 and dma to communicate rs485 at a transmission rate of 2.5mbps.

 

 

After the data is sent, it takes approximately 30 us seconds for the response to start in slave.

At this time, the first byte fills up with 0x00 intermittently, so can you suggest a solution for this?

0 件の賞賛
返信
1 返信

1,266件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @tj_P 

Can you tell me the clock speed of you MK10? 120MHz, 100MHz, 75MHz or 50MHz.

Can you provide me more details please? What do you mean with " for the response to start in slave"? UART does not uses master/slave modes.

Best Regards, Miguel.

0 件の賞賛
返信