Hello Kan,
Thanks for your reply.
Im using the Arduino IDE with the teenduino Plugin.
I use it because i have a Teensy 3.1
The teensy is microcontroller board based on MK20DX256VLH7 (Cortex-M4
base)
Because of the special IDE i think it is'nt useful if i share my code.
If i have a small sample program i can easy port.
For test if i can catch LIN messages i make a test program only with the
functionality to print out the LIN data.
The Lin protocol in my application is v1.3 / the speed is 19200.
It would be really nice if you can give me some informations.
My Serial initialisation routine is:
void serial_begin(uint32_t divisor)
{
ledVal = 0;
digitalWrite(LEDPIN, ledVal);
SIM_SCGC4 |= SIM_SCGC4_UART0; // turn on clock, TODO: use
bitband
rx_buffer_head = 0;
rx_buffer_tail = 0;
tx_buffer_head = 0;
tx_buffer_tail = 0;
transmitting = 0;
CORE_PIN0_CONFIG = PORT_PCR_PE | PORT_PCR_PS | PORT_PCR_PFE |
PORT_PCR_MUX(3);
CORE_PIN1_CONFIG = PORT_PCR_DSE | PORT_PCR_SRE | PORT
PCRMUX(3);
UART0_BDH = (divisor >> 13) & 0x1F;
UART0_BDL = (divisor >> 5) & 0xFF;
UART0_C4 = divisor & 0x1F;
//UART0_C1 = 0;
UART0_C1 = UART_C1_ILT;
UART0_TWFIFO = 2; // tx watermark, causes S1_TDRE to set
UART0_RWFIFO = 4; // rx watermark, causes S1_RDRF to set
UART0_PFIFO = UART_PFIFO_TXFE | UART_PFIFO_RXFE;
UART0_C2 = C2_TX_INACTIVE;
// #if UART_MODE == LIN_MODE
UART0_BDH = UART_BDH_LBKDIE |((divisor >> 13) & 0x1F);
UART0_BDL = (divisor >> 5) & 0xFF;
UART0_S2 = UART0_S2 | UART_S2_BRK13 | UART_S2_LBKDE;
// #endif
NVIC_SET_PRIORITY(IRQ_UART0_STATUS, IRQ_PRIORITY);
NVIC_ENABLE_IRQ(IRQ_UART0_STATUS);
}
my Interrupt service routine:
// status interrupt combines
// Transmit data below watermark UART_S1_TDRE
// Transmit complete UART_S1_TC
// Idle line UART_S1_IDLE
// Receive data above watermark UART_S1_RDRF
// LIN break detect UART_S2_LBKDIF
// RxD pin active edge UART_S2_RXEDGIF
void uart0_status_isr(void)
{
uint32_t head, newhead, tail, n;
uint8_t avail, c, buffer;
if (UART0_S2 & UART_S2_LBKDIF)
{
__disable_irq();
// if (UART_S1 & UART_S1_OR) avail =
UART0_S1;
buffer = UART0_D;
digitalWrite(OTHERPIN, ledVal ^= 1);
avail = UART0_S1;
UART0_S1 = avail;
avail = UART0_S1;
// (void)(UART0_S1 == 0); //
Dummy read of the SCIS1 register to clear flags
// (void)(UART0_D == 0); //
Dummy read of the SCID register to clear flags
if (UART0_S2 & UART_S2_LBKDIF &
UART_S2_RXEDGIF)
{
UART0_S2 = UART0_S2 |
UART_S2_LBKDIF |UART_S2_RXEDGIF ;
lin_break_count
=lin_break_count+20;
}
else UART0_S2 = (UART0_S2 |
UART_S2_LBKDIF);
lin_break_count++;
avail = UART0_RCFIFO;
if (avail == 0) {
(void)(UART0_S1 == 0);
// Dummy read of the SCIS1 register to clear flags
(void)(UART0_D == 0);
// Dummy read of the SCID register to clear flags
c = UART0_D;
UART0_CFIFO = UART_CFIFO_RXFLUSH;
__enable_irq();
}
else {
__enable_irq();
head = rx_buffer_head;
tail = rx_buffer_tail;
do {
n = UART0_D;
if (use9Bits && (UART0_C3
& 0x80)) n |= 0x100;
newhead = head + 1;
if (newhead >=
RX_BUFFER_SIZE) newhead = 0;
if (newhead != tail) {
head = newhead;
rx_buffer[head]
=
n;
}
} while (--avail > 0);
rx_buffer_head = head;
__enable_irq();
}
/* if (lin_break_count < 10000)
{
lin_break_count++;
// UART0_S2 = UART0_S2 |
UART_S2_LBKDIF ; // to clear the LIN Flag write it
c = UART0_S1;
c = c + UART0_S2;
c = c + UART0_C1;
c = c + UART0_C2;
c = c + UART0_C3;
c = c + UART0_D;
lin_break_count = UART0_RCFIFO
+c;
}
else lin_break_count = 0;
*/
}
if (UART0_S1 & (UART_S1_RDRF | UART_S1_IDLE)) {
__disable_irq();
avail = UART0_RCFIFO;
if (avail == 0) {
// The only way to clear the IDLE interrupt flag
is
// to read the data register. But reading with no
// data causes a FIFO underrun, which causes the
// FIFO to return corrupted data.
c = UART0_D;
UART0_CFIFO = UART_CFIFO_RXFLUSH;
__enable_irq();
} else {
__enable_irq();
head = rx_buffer_head;
tail = rx_buffer_tail;
do {
n = UART0_D;
if (use9Bits && (UART0_C3 & 0x80)) n |=
0x100;
newhead = head + 1;
if (newhead >= RX_BUFFER_SIZE) newhead =
0;
if (newhead != tail) {
head = newhead;
rx_buffer[head] = n;
}
} while (--avail > 0);
rx_buffer_head = head;
}
}
c = UART0_C2;
if ((c & UART_C2_TIE) && (UART0_S1 & UART_S1_TDRE)) {
head = tx_buffer_head;
tail = tx_buffer_tail;
do {
if (tail == head) break;
if (++tail >= TX_BUFFER_SIZE) tail = 0;
avail = UART0_S1;
n = tx_buffer[tail];
if (use9Bits) UART0_C3 = (UART0_C3 & ~0x40) | ((n
& 0x100) >> 2);
UART0_D = n;
} while (UART0_TCFIFO < 8);
tx_buffer_tail = tail;
if (UART0_S1 & UART_S1_TDRE) UART0_C2 = C2_TX_COMPLETING;
}
if ((c & UART_C2_TCIE) && (UART0_S1 & UART_S1_TC)) {
transmitting = 0;
if (transmit_pin) *transmit_pin = 0;
UART0_C2 = C2_TX_INACTIVE;
}
lin_break_count = buffer;
}
as you some of the code is greyed out - because i test different settings
to get it working.
I hope you can support me.
B.R:
Frank
Mit freundlichen Grüßen / best regards
Frank Münzner
E.G.O. Elektro-Gerätebau GmbH
Innovation / Research & Developement
Rote-Tor-Straße 14
75038 Oberderdingen
Deutschland
Fon +49 7045 45-68088
Fax +49 7045 9615-68088
E-Mail: Frank.Muenzner@egoproducts.com
Internet: http://www.egoproducts.com
Geschäftsführer: Dr. Johannes Haupt (Vors.), Dr. Karlheinz Hörsting
Vorsitzender des Aufsichts- u. Verwaltungsrates: Armin Sohler
Sitz: Oberderdingen, Handelsregister Mannheim HRB 240 044
Von: Kan_Li <admin@community.freescale.com>
An: Frank Muenzner <frank.muenzner@egoproducts.com>,
Datum: 10.07.2014 04:34
Betreff: Re: - How to use the Uart in
LIN Mode in Kinetis K20 Family
How to use the Uart in LIN Mode in Kinetis K20 Family
reply from Kan_Li in Kinetis Microcontrollers - View the full discussion
Hi Frank,
I will contact our local AE team to check if any sample code available for
your reference, and would you please share your code for a review? Which
IDE you are using? Please kindly help to clarify! Thanks for your
patience!
Have a great day!
B.R
Kan
Reply to this message by replying to this email, or go to the message on
Freescale Community
Start a new discussion in Kinetis Microcontrollers by email or at
Freescale Community
Following How to use the Uart in LIN Mode in Kinetis K20 Family in these
streams: Inbox