How to switch to older version of firmware in PE MICRO UNIVERSAL MULTILINK FX Rev B (PEMB1BF40)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to switch to older version of firmware in PE MICRO UNIVERSAL MULTILINK FX Rev B (PEMB1BF40)

1,710 次查看
pritampatil
Contributor III

I was using PE MICRO universal multilink FX for debugging my project. 

Ir was working fine for me until i updated my S32DS IDE and the firmware of PE MICRO universal multilink FX also got updated automatically when i tried to debug it.

Now PE MICRO universal multilink FX is not responding properly.

It is unable to enter DEBUG mode.

error1.PNG

After clicking on ABORT, i got the following message.

error2.PNG

I have re--installed the S32DS older version(the one without updates) still it is not working fine.

I think reverting back to older version of firmware may resolve the issue. If not, please suggest an alternative.

How to revert back to older version?

I have downloaded

http://www.pemicro.com/downloads/main_downloads_temp/201810031258175283381/multilink_universal_insta... 

and installed firmware given here, but it didn't work...

Please revert back ASAP.

Regards,

Pritam

0 项奖励
回复
2 回复数

1,558 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

which version of S32DS you use? Which update did you install?

We have no other similar incidents with S32DS and PeMicro debugger.

Regards,

Martin

0 项奖励
回复

1,558 次查看
pritampatil
Contributor III

S32DS version: 

S32DS_ARM_Win32_v2018.R1_b180326

Which updates did i install???

updates.PNG

But even after uninstalling the software and reinstalling it with older version(without updates), it is not working properly.

Regards,

Pritam

0 项奖励
回复