How to read and write internal EEPROM from MKE02Z16VLC4?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to read and write internal EEPROM from MKE02Z16VLC4?

3,286件の閲覧回数
julianacamargo
Contributor I

Hello,

Can someone send me the routines to read/write and erase one or more bytes on internal MKE02Z16VLC4 EEEPROM?

Thanks!

Regards,

Juliana

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,222件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Juliana Camargo,

     About the KE02 eeprom operation routine, you can refer to the KE02 reference manual.​​

Chapter 18 Flash Memory Module (FTMRH)

    Besides, we have the according sample code for KE02 EEPROM, the code download link is:FRDM-KEXX Driver Library Package

Code folder path is:KEXX_DRIVERS_V1.2.1_DEVD\kexx_drv_lib\build\iar\ke02\EEPROM_demo

Wish it helps you!

If you still have question, please contact with me!

Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,222件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The following article explains the EEPROM: http://www.utasker.com/kinetis/KE_EEPROM.html

It is supported in the uTasker KE02 project in case you would prefer a complete solution with simulation capability of the chip (including EEPROM) and for your complete project.

I have attached the flash driver which supports KE, K flash and KE EEPROM so that you can also just take snippets otherwise - search for reference {109} for code handling KE EEPROM.

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html

KE: http://www.utasker.com/kinetis/FRDM-KE02Z.html / http://www.utasker.com/kinetis/FRDM-KE02Z40M.html / http://www.utasker.com/kinetis/FRDM-KE04Z.html / http://www.utasker.com/kinetis/FRDM-KE06Z.html

Serial Bootloader for KE02/KE04/KE06 (KBOOT, AN2295, SREC, SD-card): http://www.utasker.com/forum/index.php?topic=1873.msg6796#msg6796 / http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.PDF</p>

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 件の賞賛
返信