Hi,
There is an application note AN4373 about how to get more accuracy ADC measurement of Kinetis ADC module.
More detailed info, please check below link:
http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4373.pdf
As you mentioned ADC module do calibration before measurement, please check below suggestions how to get more better performance:
*All digital I/Os should be silent,
*Unnecessary modules should be disabled
*VREFH should be stable and high voltage as possible (higher ADC code widths)
*isolated VREFH would be an ideal
*The ADC clock should be as noise free as possible (low jitter – PLL, FLL, OSC)
*Hardware averaging should be set to maximum (32 samples)
*Low power conversion should be disabled
*Do the calibration at room temperature
So far, Kinetis datasheet without ADC module temp drift refer info.
The ADC measurement temperature drift also could be affected by ADC reference voltage, please check the ADC reference voltage value during the measurement.
Wish it helps.
best regards
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------