How to import baremetal example in kinetis design studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to import baremetal example in kinetis design studio

2,353件の閲覧回数
sameerarvikar
Contributor III

I am using kinetis design studio v3.2 and kinetis k70

I downloaded baremetal examples for kinetis k70 from the following link

https://www.nxp.com/webapp/sps/download/preDownload.jsp 

I imported the projects(e.g. helloworld)from the directory downloaded from above link as given in kinetis design studio user guide

Now if i build the project

Following warning comes  :-   Invalid project path: Include path not found (some path).

when i go to project properties 

project > properties > c/C++ Build > Settings

I found following error

Orphaned configuration. No base extension cfg exists for com.freescale.arm.cdt.toolchain.config.arm.release.2020066743

so i followed the steps given on following page (Steps of the conversion by manual configuration of the toolchain)

CW MCU 10.6 Processor Expert projects migration into KDS 3.0.0 

Now the following error is coming for helloworld example

fatal error: common.h: No such file or directory hello_world.c /k70-hello-world/Sources/hello_world line 7 C/C++ Problem


make: *** [Sources/hello_world/hello_world.o] Error 1 k70-hello-world C/C++ Problem

how to resolve the problem

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,033件の閲覧回数
sameerarvikar
Contributor III

I also tried the following document

http://www.nxp.com/assets/documents/data/en/user-guides/KDSPUG.pdf 

but no dialog box apears after i click on  Convert CodeWarrior project file..

0 件の賞賛
返信

2,033件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello sameer,

I don't recommend you use the directly porting, because there always some error need to configuration.

You  can create a new project on KDS, then  copy the the function files from CW to KDS project , build ,

even there is error , it easy to find and fix.

It seems you just want use KDS to develop K70,  so I recommend you can create Processor Expert project

on KDS, there is also example , they can directly run on KDS :

- When create project  ,please choose "Processor Expert" :

pastedImage_1.png

- For example , you want configuration a GPIO,  just double click "GPIO_LDD" , it will add to your project :

pastedImage_2.png

- Then click "help on component " -> Typical Usage :

pastedImage_3.png

pastedImage_4.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,033件の閲覧回数
sameerarvikar
Contributor III

Thanks,

I also tried codewarrior or mcu v10.7 , there also errors were coming

0 件の賞賛
返信