How to create lib files with codewarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to create lib files with codewarrior

ソリューションへジャンプ
4,594件の閲覧回数
jimtom
Contributor I

How to create lib files with codewarrior

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
4,311件の閲覧回数
BlackNight
NXP Employee
NXP Employee
0 件の賞賛
返信
6 返答(返信)
4,311件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

with MCU10.3 there is library option available in the wizard.

Otherwise: see

Creating and using Libraries with ARM gcc and Eclipse | MCU on Eclipse

I hope this helps.

0 件の賞賛
返信
4,311件の閲覧回数
jimtom
Contributor I

not found library option available in the wizard

0 件の賞賛
返信
4,311件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Have you selected a Kinetis device?

It is available for me both in MCU10.4 and MCU10.3.

Maybe you are using an older version?

0 件の賞賛
返信
4,311件の閲覧回数
jimtom
Contributor I

I use MCU10.3.

0 件の賞賛
返信
4,311件の閲覧回数
jimtom
Contributor I

not found library option available in the wizard

1.JPG

0 件の賞賛
返信
4,311件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Select 'Bareboard project' and then it is here:

http://mcuoneclipse.files.wordpress.com/2013/02/library-creation.png

0 件の賞賛
返信