Hi Siva,
You have many good questions. I will try to answer but will also ask a few questions too.
To start with which Kinetis device best fit your initial need (ex: K10/K20/K40/K60/K70)?
Which development tools are you using (ex: CW10.6/IAR/Keil/Other)?
Do you want a full RTOS (like MQX) or a simpler smaller RTOS (like MQXLite) or baremetal?
Will you require higher level peripherals like Ethernet, or USB, or access to SDCard or, Other?
To answer your questions:
Q1. Where to check for the registers to be configure according to the project need ?
A1. All Kinetis devices have Reference Manuals that describe the specific peripheral implementation and this is usually in Chapter 3. The actual signal pinout is in Chapter 10. Please note that with such highly integrated MCU's most pins have more than one function. Chapter 10 will show you what peripheral options you have for each pin. With that said on high pin count devices, a UART0 might be able to be configured to come out on different pins. Note you can only direct it to one set of pins and not all options. This is the manual approach. A more automated approach would be to use the standalone PExDrv10.4 (Processor Expert-PE) eclipse GUI based tool or the PE tool integrated into CW10.6. PE can help you decide which pins to use for the different peripheral you want to use.
Q2. Or How to know where the Registers are configured ?
A2. The MCU/device Reference Manual has all peripheral register definitions and default (POR-Power On Reset) configurations. Kinetis devices in general start up (POR) in a low power state with most peripheral modules disabled, using internal clock and GPIO pins set to GPIO inputs. It is the software (baremetal or MQX or MQXLite or PE code) that will initialize the MCU/device and ramp your clock up to desired frequency.
Q3. How to configure the individual pins of the Microcontroller through MQX ?
A4. MQX has many examples in the freely downloaded distribution (www.freescale.com/mqx) . The default install directory with lots of great examples:
C:\Freescale\Freescale_MQX_4_1_0_GA\mqx\examples
Specifically the GPIO example is at:
C:\Freescale\Freescale_MQX_4_1_0_GA\mqx\examples\gpio
Optionally you could use PE and its GPIO components to access individual pins too.
Q4. Or Tell me how the Pins are configured in MQX RTOS ?
A4. Please study the GPIO example mentioned in A4.
Other Notes:
Each MCU/device product page has a wealth of information from documents to schematics to baremetal example code and more.
I usually
Useful web links:
www.freescale.com/mqx MQX download and resources.
www.freescale.com/kinetis access to entire family of Kinetis MCUs...and eventually MCD/device product page to get docs
www.freescale.com/processorexpert GUI initialization, driver software generation, auto-code generating
www.freescale.com/tower rapid prototyping kit but cost more
www.freescale.com/freedom in-expensive development kit
www.freescale.com/ftf FTF is Freescale awesome customer only technical training event over multiple days in various locations around the world that give hands-on training, many example application demos', 3rd party vendors, and much more. The Americas link (FTF America happened in April 2014) has many of the training classes online. Check out the following link:
Freescale Technical Sessions Library|Freescale
Hope this helps.
Regards,
David