How to configure PWM offset on MKE14F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure PWM offset on MKE14F

Jump to solution
3,591 Views
kwf
Contributor III

Hi Community

Do the MKE14F FTM_PWM can achieve PWM offset function?

The PWM2 offset Ts/2 than PWM1.

kwf_0-1639375626341.png

 

 

 

0 Kudos
Reply
1 Solution
3,577 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello @kwf ,

The PWM of the MKE14 can achieve this offset configuration there is no limitation mentioned for this product in the documentation. But this type of configuration does not have an specific function either an SDK example. Please let me know if you have any other question or if I can help you on anything else.

View solution in original post

0 Kudos
Reply
3 Replies
3,578 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello @kwf ,

The PWM of the MKE14 can achieve this offset configuration there is no limitation mentioned for this product in the documentation. But this type of configuration does not have an specific function either an SDK example. Please let me know if you have any other question or if I can help you on anything else.

0 Kudos
Reply
3,571 Views
kwf
Contributor III

Hi nxf77486

Is it combine mode? How to configure those register?

Which section in documentation mention PWM offset?

In "Kinetis KE1xF Sub-Family Reference Manual, Rev. 4, 06/2019" 41.5.9 Combine mode 

The channel out put will reset to initial status (High or low depend on ELSB and ELSA register) when count to MOD value. No matter what, the out put is not offset. Did I misunderstand?

0 Kudos
Reply
3,556 Views
kwf
Contributor III

Hi 

I found solution.

Thanks for help!

0 Kudos
Reply