How to communicate between two FRDM K64F boards using UART?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to communicate between two FRDM K64F boards using UART?

1,880件の閲覧回数
siddharthpimpri
Contributor II

FRDM-K64F

0 件の賞賛
返信
1 返信

1,443件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Customer can select to use below pins for UART communication:

PTE8      UART5_TX          J1-13

PTE9     UART5_RX          J1-9

PTE24     UART4_TX         J2-13

PTE25     UART4-RX          J2-15


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------