How to communicate between two FRDM K64F boards using UART?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to communicate between two FRDM K64F boards using UART?

1,802 Views
siddharthpimpri
Contributor II

FRDM-K64F

0 Kudos
Reply
1 Reply

1,365 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Customer can select to use below pins for UART communication:

PTE8      UART5_TX          J1-13

PTE9     UART5_RX          J1-9

PTE24     UART4_TX         J2-13

PTE25     UART4-RX          J2-15


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------