How to calculate the delay time of the Programmable Delay Block (PDB)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to calculate the delay time of the Programmable Delay Block (PDB)?

1,555 Views
小勇邹
Contributor II

Hi,

How to calculate the delay time of the Programmable Delay Block (PDB) in KM34?

For example, if setting PDB0_CH0DLY0=200, how to calculate the delay time?

And I cannot find the clock source for PDB in the data sheet. Can you also tell me the clock source of PDB?

Labels (1)
0 Kudos
Reply
1 Reply

1,271 Views
AleGuzman
NXP Employee
NXP Employee

The PDB clock reference can be found at the KM34 Reference Manual Chapter 5 Clock Distribution 

pastedImage_1.png

To calculate a PDB channel delay you need to use the configurable PDB registers bits:

PDB Clock = Bus Clock / ( Preescaler x Mult )

Preescaler -- PDBx_SC[PREESCALER]

pastedImage_6.png

Mult -- PDBx_SC[MULT]

pastedImage_7.png

Channel Delay = PDB Clock / PDBx_CHnDLY0  

For example
Bus Clock = 24 MHz

Preescaler = 011 (8 times) 

Mult = 01 ( factor is 10 )

PDBx_CHnDLY0 = 300 

PDB Clock = 24 MHz / ( 8 x 10 ) = 300 kHz            1 PDB Count = 3.33 us

Channel Delay = 300 kHz / 300 = 1 kHz                  Channel timer = 1 ms

0 Kudos
Reply