How to Program custom board's MK20dx128vll7 microcontroller using TWRk20d72M Devlopment Board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to Program custom board's MK20dx128vll7 microcontroller using TWRk20d72M Devlopment Board?

1,056 Views
parthmodi
Contributor I

Hello,

I have TWRK20D72M EVM Board and I want to program and debug MK20DX128VLL7 microcontroller.I have my own custom board.

I used the SWD interface for the programming the controller.I used the TWDK20D72M 's J11 port for the programming the MK20dx128vll7.

I have below listed queries for the same.

1) Is it possible to progarm and debug the MK20DX128LL7 controller use of TWEK20D72M.

2) If yes than,how???

Any help in this case would be great appreciated

Please let me know if you need more information from the our side.

Thanks,

Parth Modi

0 Kudos
Reply
0 Replies