How SMBUS slave device detect a STOP signal from the master?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How SMBUS slave device detect a STOP signal from the master?

12,552件の閲覧回数
alvenwu
Contributor I

HI

I am using Kenitis K10 Cortex m4 CPU on our board , when it was taken as a  SMBUS slave device .

I checked all the registers of I2C and SMBUS  , but still cannot find how this slave device check whether it is the final byte in the transfer from the master device, when it is in receive slave mode.

Could you know which bit in the registers means the slave device receives a stop signal? and would the STOP signal issue a individual interrupt ? 

thanks  a lot.

ラベル(2)
0 件の賞賛
返信
22 返答(返信)

820件の閲覧回数
alvenwu
Contributor I

HI Mike

no , I didn't set this bit. Actually I cleared it , which also mean I don't need to set the I2C slave clock frequency ,just following the master's transfer speed.

And I set this bit , does it mean i also set the slave clock frequency , and SCL stretching disable?

thanks

best Regards

Alven

0 件の賞賛
返信

821件の閲覧回数
alvenwu
Contributor I

hi , who can give any advice ?  and can we design a slave smbus device driver?

0 件の賞賛
返信