Hi, could you kindly recommend the micro controller series which have been used for vehicle to Grid (V2G) Application.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi, could you kindly recommend the micro controller series which have been used for vehicle to Grid (V2G) Application.

3,003 Views
suriyaprakasamc
Contributor I

Hi,

could you kindly recommend the specific micro controller series which have been used for vehicle to Grid (V2G) Application.

Regards,

Suriyaprakasam C

0 Kudos
Reply
5 Replies

2,905 Views
suriyaprakasamc
Contributor I

Hi Jing,

We are Looking for micro controller series which is already used in  Electric Vehicle communication controller (EVCC) for DC level 2 charger application.

Please, let me know if any other clarifications.

Thanks & Regards,

Suriyaprakasam C

0 Kudos
Reply

2,905 Views
suriyaprakasamc
Contributor I

Hi Jing,

We are Looking for micro controller series which is already used in  Electric Vehicle communication controller (EVCC) for DC level 2 charger application.

Please, consider below preliminary specifications for selection of controller also indicate the availability of evaluation board.

Core Type : Dual Core

Flash Memory : 2-4MB

Operating Frequency : 150 -200MHz

Functional Safety – ISO26262(ASILD(or) B)

CAN – 3 Channels

SPI – 3 Channels

UART – 3 Channels

Ethernet –1 Channel (Min)

Operating Temperature –(-40 to 125C)

Supply Voltage -3.3V

AEC Qualified

Thanks & Regards,

Suriyaprakasam C

0 Kudos
Reply

2,905 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

take a look at this one, it should fit your needs:

MPC574xB/C/G|32-bit MCU|Gateway|NXP 

Regards,

Lukas

0 Kudos
Reply

2,905 Views
suriyaprakasamc
Contributor I

Hi Lukas,

Thanks for your support

Can you suggest alternate for 5748G because it is too costly. please, specify if any special controller series available in Nxp for Electric Vehicle communication controller ECU in Dc level 2 Application(V2G).

Thanks,

Suriyaprakasam

0 Kudos
Reply

2,905 Views
jingpan
NXP TechSupport
NXP TechSupport

Dear Suriyaprakasam,

I think when we tall about V2G, that is a big system, include power management, communication, metering and measurement. So can you give some detail information about what you want.

http://www.nxp.com/applications/internet-of-things/smart-things/smart-energy/off-grid-solar-power-in...

0 Kudos
Reply